Unable to connect to target device - STM32H7S3L8H6 (NUCLEO-H7S3L8)
Dear all,
I have purchased the NUCLEO-H7S3L8. I am facing an issue when trying to debug a basic (blank) project. The Debugger is unable to connect to the target. Here is the console output :
"
STMicroelectronics ST-LINK GDB server. Version 7.10.0
Copyright (c) 2025, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_fldzzj.log
ST-LINK SN : 0020002B3433511830343835
ST-LINK FW : V3J16M7
Board : NUCLEO-H7S3L8
Voltage : 3,30V
SWD freq : 8000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x485
Revision ID : Rev B
Device name : STM32H7RSxx
Flash size : 64 KBytes (default)
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0xE4
Opening and parsing file: ST-LINK_GDB_server_YZEder.srec
Memory Programming ...
File : ST-LINK_GDB_server_YZEder.srec
Size : 6.39 KB
Address : 0x08000000
Erasing memory corresponding to sector 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.057
-------------------------------------------------------------------
STM32CubeProgrammer v2.19.0
-------------------------------------------------------------------
Log output file: /tmp/STM32CubeProgrammer_MGG0Vd.log
Error: Unable to connect to the target device, Access port is not valid.
Encountered Error when opening /opt/st/stm32cubeide_1.18.1/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.linux64_2.2.100.202412061334/tools/bin/STM32_Programmer_CLI
Error in STM32CubeProgrammer
Shutting down...
Exit.
"
The project I am trying to debug is the standard code generated when creating a new project in STM32CubeIDE. The only thing I changed is the Debugger Configuration (I changed it iaw this guide : https://community.st.com/t5/stm32-mcus/stm32cubeide-how-to-debug-an-stm32h7rx-sx-project-without/ta-p/737120).
I have already tried a mass erase (using the BOOT0 pin and STM32 Programmer) but the issue persists.
Can someone assist me on how to launch a Debug session (even from an Example project) with the NUCLEO-H7S3L8 ?