unable to run the readily given example from mx for stm326570-dk nx_webserver_project

I am trying to build the readily given Nx_webserver project , i had selected the given example and just change the tool chain to STMcube IDE inorder to build the project with the cube ide after redirection to the cube IDE i just click on the build , it ends up with the following error:
12:03:20 **** Build of configuration Debug for project Nx_WebServer_FSBL ****
make -j8 all
arm-none-eabi-gcc "C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_block_pool_performance_info_get.c" -mcpu=cortex-m55 -std=gnu11 -g3 -DRTL8211_INIT_TO=10000 -DETH_PHY_1000MBITS_SUPPORTED -DDEBUG -DUSE_HAL_DRIVER -DSTM32N657xx -DFX_INCLUDE_USER_DEFINE_FILE -DNX_INCLUDE_USER_DEFINE_FILE -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_SECURE=1 -c -I../../../Middlewares/ST/netxduo/ports/cortex_m55/gnu/inc -I../../../Middlewares/ST/threadx/ports/cortex_m55/gnu/inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -mcmse -MMD -MP -MF"Middlewares/threadx/Performance/tx_block_pool_performance_info_get.d" -MT"Middlewares/threadx/Performance/tx_block_pool_performance_info_get.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/threadx/Performance/tx_block_pool_performance_info_get.o"
arm-none-eabi-gcc "C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_block_pool_performance_system_info_get.c" -mcpu=cortex-m55 -std=gnu11 -g3 -DRTL8211_INIT_TO=10000 -DETH_PHY_1000MBITS_SUPPORTED -DDEBUG -DUSE_HAL_DRIVER -DSTM32N657xx -DFX_INCLUDE_USER_DEFINE_FILE -DNX_INCLUDE_USER_DEFINE_FILE -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_SECURE=1 -c -I../../../Middlewares/ST/netxduo/ports/cortex_m55/gnu/inc -I../../../Middlewares/ST/threadx/ports/cortex_m55/gnu/inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -mcmse -MMD -MP -MF"Middlewares/threadx/Performance/tx_block_pool_performance_system_info_get.d" -MT"Middlewares/threadx/Performance/tx_block_pool_performance_system_info_get.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/threadx/Performance/tx_block_pool_performance_system_info_get.o"
arm-none-eabi-gcc "C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_byte_pool_performance_info_get.c" -mcpu=cortex-m55 -std=gnu11 -g3 -DRTL8211_INIT_TO=10000 -DETH_PHY_1000MBITS_SUPPORTED -DDEBUG -DUSE_HAL_DRIVER -DSTM32N657xx -DFX_INCLUDE_USER_DEFINE_FILE -DNX_INCLUDE_USER_DEFINE_FILE -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_SECURE=1 -c -I../../../Middlewares/ST/netxduo/ports/cortex_m55/gnu/inc -I../../../Middlewares/ST/threadx/ports/cortex_m55/gnu/inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -mcmse -MMD -MP -MF"Middlewares/threadx/Performance/tx_byte_pool_performance_info_get.d" -MT"Middlewares/threadx/Performance/tx_byte_pool_performance_info_get.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/threadx/Performance/tx_byte_pool_performance_info_get.o"
arm-none-eabi-gcc "C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_byte_pool_performance_system_info_get.c" -mcpu=cortex-m55 -std=gnu11 -g3 -DRTL8211_INIT_TO=10000 -DETH_PHY_1000MBITS_SUPPORTED -DDEBUG -DUSE_HAL_DRIVER -DSTM32N657xx -DFX_INCLUDE_USER_DEFINE_FILE -DNX_INCLUDE_USER_DEFINE_FILE -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_SECURE=1 -c -I../../../Middlewares/ST/netxduo/ports/cortex_m55/gnu/inc -I../../../Middlewares/ST/threadx/ports/cortex_m55/gnu/inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -mcmse -MMD -MP -MF"Middlewares/threadx/Performance/tx_byte_pool_performance_system_info_get.d" -MT"Middlewares/threadx/Performance/tx_byte_pool_performance_system_info_get.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/threadx/Performance/tx_byte_pool_performance_system_info_get.o"
arm-none-eabi-gcc "C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_event_flags_performance_info_get.c" -mcpu=cortex-m55 -std=gnu11 -g3 -DRTL8211_INIT_TO=10000 -DETH_PHY_1000MBITS_SUPPORTED -DDEBUG -DUSE_HAL_DRIVER -DSTM32N657xx -DFX_INCLUDE_USER_DEFINE_FILE -DNX_INCLUDE_USER_DEFINE_FILE -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_SECURE=1 -c -I../../../Middlewares/ST/netxduo/ports/cortex_m55/gnu/inc -I../../../Middlewares/ST/threadx/ports/cortex_m55/gnu/inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -mcmse -MMD -MP -MF"Middlewares/threadx/Performance/tx_event_flags_performance_info_get.d" -MT"Middlewares/threadx/Performance/tx_event_flags_performance_info_get.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/threadx/Performance/tx_event_flags_performance_info_get.o"
arm-none-eabi-gcc "C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_event_flags_performance_system_info_get.c" -mcpu=cortex-m55 -std=gnu11 -g3 -DRTL8211_INIT_TO=10000 -DETH_PHY_1000MBITS_SUPPORTED -DDEBUG -DUSE_HAL_DRIVER -DSTM32N657xx -DFX_INCLUDE_USER_DEFINE_FILE -DNX_INCLUDE_USER_DEFINE_FILE -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_SECURE=1 -c -I../../../Middlewares/ST/netxduo/ports/cortex_m55/gnu/inc -I../../../Middlewares/ST/threadx/ports/cortex_m55/gnu/inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -mcmse -MMD -MP -MF"Middlewares/threadx/Performance/tx_event_flags_performance_system_info_get.d" -MT"Middlewares/threadx/Performance/tx_event_flags_performance_system_info_get.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/threadx/Performance/tx_event_flags_performance_system_info_get.o"
arm-none-eabi-gcc "C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_mutex_performance_info_get.c" -mcpu=cortex-m55 -std=gnu11 -g3 -DRTL8211_INIT_TO=10000 -DETH_PHY_1000MBITS_SUPPORTED -DDEBUG -DUSE_HAL_DRIVER -DSTM32N657xx -DFX_INCLUDE_USER_DEFINE_FILE -DNX_INCLUDE_USER_DEFINE_FILE -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_SECURE=1 -c -I../../../Middlewares/ST/netxduo/ports/cortex_m55/gnu/inc -I../../../Middlewares/ST/threadx/ports/cortex_m55/gnu/inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -mcmse -MMD -MP -MF"Middlewares/threadx/Performance/tx_mutex_performance_info_get.d" -MT"Middlewares/threadx/Performance/tx_mutex_performance_info_get.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/threadx/Performance/tx_mutex_performance_info_get.o"
arm-none-eabi-gcc "C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_mutex_performance_system_info_get.c" -mcpu=cortex-m55 -std=gnu11 -g3 -DRTL8211_INIT_TO=10000 -DETH_PHY_1000MBITS_SUPPORTED -DDEBUG -DUSE_HAL_DRIVER -DSTM32N657xx -DFX_INCLUDE_USER_DEFINE_FILE -DNX_INCLUDE_USER_DEFINE_FILE -DTX_INCLUDE_USER_DEFINE_FILE -DTX_SINGLE_MODE_SECURE=1 -c -I../../../Middlewares/ST/netxduo/ports/cortex_m55/gnu/inc -I../../../Middlewares/ST/threadx/ports/cortex_m55/gnu/inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -fcyclomatic-complexity -mcmse -MMD -MP -MF"Middlewares/threadx/Performance/tx_mutex_performance_system_info_get.d" -MT"Middlewares/threadx/Performance/tx_mutex_performance_system_info_get.o" --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -o "Middlewares/threadx/Performance/tx_mutex_performance_system_info_get.o"
C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_block_pool_performance_info_get.c:28:10: fatal error: tx_api.h: No such file or directory
28 | #include "tx_api.h"
| ^~~~~~~~~~
compilation terminated.
C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_block_pool_performance_system_info_get.c:28:10: fatal error: tx_api.h: No such file or directory
28 | #include "tx_api.h"
| ^~~~~~~~~~
compilation terminated.
C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_byte_pool_performance_info_get.c:28:10: fatal error: tx_api.h: No such file or directory
28 | #include "tx_api.h"
| ^~~~~~~~~~
compilation terminated.
C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_event_flags_performance_system_info_get.c:28:10: fatal error: tx_api.h: No such file or directory
28 | #include "tx_api.h"
| ^~~~~~~~~~
compilation terminated.
C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_byte_pool_performance_system_info_get.c:28:10: fatal error: tx_api.h: No such file or directory
28 | #include "tx_api.h"
| ^~~~~~~~~~
compilation terminated.
make: *** [Middlewares/threadx/Performance/subdir.mk:64: Middlewares/threadx/Performance/tx_block_pool_performance_info_get.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Middlewares/threadx/Performance/subdir.mk:68: Middlewares/threadx/Performance/tx_byte_pool_performance_info_get.o] Error 1
make: *** [Middlewares/threadx/Performance/subdir.mk:66: Middlewares/threadx/Performance/tx_block_pool_performance_system_info_get.o] Error 1
C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_event_flags_performance_info_get.c:28:10: fatal error: tx_api.h: No such file or directory
28 | #include "tx_api.h"
| ^~~~~~~~~~
compilation terminated.
make: *** [Middlewares/threadx/Performance/subdir.mk:74: Middlewares/threadx/Performance/tx_event_flags_performance_system_info_get.o] Error 1
make: *** [Middlewares/threadx/Performance/subdir.mk:70: Middlewares/threadx/Performance/tx_byte_pool_performance_system_info_get.o] Error 1
make: *** [Middlewares/threadx/Performance/subdir.mk:72:
Middlewares/threadx/Performance/tx_event_flags_performance_info_get.o] Error 1
C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_mutex_performance_info_get.c:28:10: fatal error: tx_api.h: No such file or directory
28 | #include "tx_api.h"
| ^~~~~~~~~~
compilation terminated.
C:/Users/admin/STM32Cube/Example/Nx_WebServer/Middlewares/ST/threadx/common/src/tx_mutex_performance_system_info_get.c:28:10: fatal error: tx_api.h: No such file or directory
28 | #include "tx_api.h"
| ^~~~~~~~~~
compilation terminated.
make: *** [Middlewares/threadx/Performance/subdir.mk:76: Middlewares/threadx/Performance/tx_mutex_performance_info_get.o] Error 1
make: *** [Middlewares/threadx/Performance/subdir.mk:78: Middlewares/threadx/Performance/tx_mutex_performance_system_info_get.o] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
12:03:22 Build Failed. 17 errors, 0 warnings. (took 2s.319ms)