USART Bootloader get checksum command doesn't work
Hello,
I am using the STM32G070RB and can start the bootloader. I am sending the command get checksum 0xA1 + 0x5E but I receive a NACK Byte directly after that. So I assume that this has to do with the protection active, since the flow diagram in the AN3155 shows only this path.
So in order to fix this issue I was thinking to send the readout unprotect command first and then the get checksum command. I did this but it doesn't work either.
Please note that I pull the Boot0 Pin high again an I am able to start the bootloader again after the reset caused by readout unprotect command.
Any help would be appreciated