USBx CDC ACM Dual Composite not working on STM32H723
Hello all,
Following up on https://community.st.com/t5/stm32cubeide-mcus/usbx-dual-composite-cdc-acm-not-working/td-p/708277, I tried to implement the same Dual CDC-ACM on STM32H723 Nucleo. I have run into the same issues.
With just one CDC_ACM class registration, the example works well. But when two classes are registered, it is gibberish on the COM port (UART).
uint8_t UserClassInstance[USBD_MAX_CLASS_INTERFACES] = {
CLASS_TYPE_CDC_ACM,
CLASS_TYPE_CDC_ACM
};
Similar to the previous post, I have modified ux_device_descriptors.c to correctly add the endpoints to the device framework string. With this change, I am able to see two ACM devices on Linux.
[ +5.485446] usb 1-4.3.2: new full-speed USB device number 48 using xhci_hcd
[ +0.191080] usb 1-4.3.2: New USB device found, idVendor=0483, idProduct=5740, bcdDevice= 2.00
[ +0.000006] usb 1-4.3.2: New USB device strings: Mfr=1, Product=2, SerialNumber=3
[ +0.000002] usb 1-4.3.2: Product: STM32 Virtual ComPort
[ +0.000002] usb 1-4.3.2: Manufacturer: STMicroelectronics
[ +0.000001] usb 1-4.3.2: SerialNumber: CDC_ACM001
[ +0.015570] cdc_acm 1-4.3.2:1.0: ttyACM1: USB ACM device
[ +0.000352] cdc_acm 1-4.3.2:1.2: ttyACM2: USB ACM device
I have also increased FIFO sizes.
VOID USBX_APP_Device_Init(VOID)
{
/* USER CODE BEGIN USB_Device_Init_PreTreatment_0 */
/* USER CODE END USB_Device_Init_PreTreatment_0 */
/* USB_OTG_HS init function */
MX_USB_OTG_HS_PCD_Init();
/* USER CODE BEGIN USB_Device_Init_PreTreatment_1 */
/* Set Rx FIFO */
HAL_PCDEx_SetRxFiFo(&hpcd_USB_OTG_HS, 0x200);
/* Set Tx FIFO 0 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 0, 0x40);
/* Set Tx FIFO 2 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 1, 0x40);
/* Set Tx FIFO 3 */
HAL_PCDEx_SetTxFiFo(&hpcd_USB_OTG_HS, 2, 0x40);
/* USER CODE END USB_Device_Init_PreTreatment_1 */
/* Initialize and link controller HAL driver */
ux_dcd_stm32_initialize((ULONG)USB_OTG_HS, (ULONG)&hpcd_USB_OTG_HS);
/* Start the USB device */
HAL_PCD_Start(&hpcd_USB_OTG_HS);
/* USER CODE BEGIN USB_Device_Init_PostTreatment */
/* USER CODE END USB_Device_Init_PostTreatment */
}
Please find the GitHub repo here.
Can someone from STM assist me please?
Best regards,
Navin