Using Stop or Standby Mode on STM32L072 (Murata CMWX1ZZABZ-078) Without External RTC
Hello,
I am working with the CMWX1ZZABZ-078 Murata module, which includes the STM32L072 MCU. I want to implement low-power modes to reduce current consumption.
Specifically, I am interested in using either Stop mode or Standby mode. However, I would like to know if it is possible to enter these modes without having an external RTC connected.
Is it mandatory to use an external RTC to wake up the MCU from these modes, or can it be done using internal clocks or other peripherals?
Any guidance or examples would be greatly appreciated.
Thank you!