Validation on target falling on F4 Discovery
Hi,
I'im running X-CUBE-AI with STM32Cube IDE on a F407 Discovery. When I try to perform validatation on target, I get the following error during building stage :
Building project
/opt/st/stm32cubeide_1.18.1/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.linux64_1.0.0.202410170706/tools/bin/arm-none-eabi-gcc -c -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -DDEBUG -DUSE_HAL_DRIVER -DSTM32F407xx -D -IMiddlewares/ST/AI/Inc -IDrivers/STM32F4xx_HAL_Driver/Inc -IDrivers/STM32F4xx_HAL_Driver/Inc/Legacy -IDrivers/CMSIS/Device/ST/STM32F4xx/Include -IDrivers/CMSIS/Include -IInc -O3 -Wall -fdata-sections -ffunction-sections Src/system_stm32f4xx.c -o Debug/Src/system_stm32f4xx.o
<command-line>: error: macro names must be identifiers
make: *** [Makefile:72: Debug/Src/system_stm32f4xx.o] Error 1
Automatic build and run failed
The project builds correctlly, but fails on validation on target. Any advices ?
Thanks,
Paulo