Question
What is the correct setup to use multiple st-links for debugging with stm32cube ide?
I'm working on a project to connect multiple stm32-boards using the CAN-bus.
So I opened two instances of the ide and connected 2 boards with 2 st-links.
When I tried to setup the 2nd st-link for debug, I received an unknown error from the GDB-server.
Please help, as I don't want to use multiple computers for that project.
Regards
Andreas