Cannot get Cube Monitor to connect to STM32G431CB on |BG431B-ESC1 board - not connected ! Unknown JTAG chain (16)
I have successfully built and downloaded the motor control application using ST motor control workbench and the CubeIDE etc and can connect to flash and step through my program. However when it comes to using CubeMonitor i get an error giving "not connected ! Unknown JTAG chain (16)"

In the config screen i can flash the LED on the board ...

I have tried both protocols SWD and and JTAG .. Can i use monitor with the BG431B-ESC1 board ?
Many thanks if youve got this far ....