Error trying to find "isTCPAvailable" when running STM32CubeMonitor in TCP mode
I'm using JetBrains CLion to debug my STM32 project, and it runs `ST-LINK_gdbserver` when debugging, and passes the "--shared" flag for other STM apps to connect into. It starts up okay, and shows "Info : default port : 7184".
I've changed my "settings.js" file in "~/.STMicroelectronics/stm32cubemonitor/" folder so that "connectionType" is "tcp" and not "p2p".
I run stm32cubemonitor, and then node-red is showing up an error of:
Cannot read properties of undefined (reading 'isTcpAvailable') (line:59)

I think this code underneath is all bundled into the distributable, so I can't debug what's actually going wrong.
The versions I have installed currently are:
ii st-stm32cubeide-2.0.0 2.0.0-26820-20251114-1348-1 amd64 IDE for STM32
ii stm32cubemonitor 1.12.0 amd64 STM32CubeMonitor helps debug a...
ii st-stlink-server 2.1.1-1 amd64 stlink tcp server to permit sev...I'm using an ST-Link/V2 ISOL
Running on Ubuntu 25.10.
Any ideas how to fix this, or where the source code is for that node-red module, or if it's a known error. Can't find any mention of this.