Skip to main content
Lep
Senior
November 14, 2022
Question

My chart crashes, I want the chart to only display the data of the last 30s, and the rest of the data is not needed. I'm testing the timestamp is achievable, but it won't work on the serial port.

  • November 14, 2022
  • 1 reply
  • 523 views

This is a serial input, the data volume per second is 12000bytes (1k Sampling rate*4channel*3bytes (single-channel sampling data size)). The input content of the serial port is as follows (part of the picture is intercepted) :0693W00000WICyMQAX.pngserial port output format: 3 bytes data + 'comma'

The procedure is as follows:

This topic has been closed for replies.

1 reply

Lep
LepAuthor
Senior
November 14, 2022

The code is to long, I can't insert it. 0693W00000WID0mQAH.png0693W00000WID1fQAH.png0693W00000WID2JQAX.png0693W00000WID2EQAX.png