Skip to main content
stephane.legargeant
ST Employee
October 1, 2021
Solved

STM32CubeMonitor v1.3.0 is available

  • October 1, 2021
  • 1 reply
  • 859 views

Hello

The new version 1.3.0 of STM32CubeMonitor is available on st.com.

You can download it on https://www.st.com/en/development-tools/stm32cubemonitor.html

Click on "Get latest" to download the version 1.3.0.

What are the changes in this version ?

  • We have updated node-RED : STM32CubeMonitor is now based on the version node-RED 1.3.7 , with dashboard 2.29.0. Other dependencies have also been updated to have an consistent package.

  • Many users have raised question about CSV export. We have proposed some solutions using node-RED nodes. (wiki export csv) This is very flexible, but need to add many nodes in the flow. So we have added an option to save the data directly in csv format in the processing node :0693W00000FB93kQAD.png

It is now very easy to export data in csv format.

  • Some users would like to be notified in the dashboard when the symbol file has changed. (symbol file = .elf .axf .out....) There is now a new output on the variable node which can be used to connect a notification box. When the file has changed, the tool will parse the symbol in background. If the symbol monitored have changed, a warning message will be sent on the new output and can be displayed in dashboard.

0693W00000FB9DBQA1.png 

  • Performance improvement : The priority of windows process has been tuned to improve the acquisition regularity.

Do not hesitate to ask questions or discuss some changes in the forum : it is a very helpful for the team to know what you need or what could be improved.

We hope the you will enjoy the changes in the new version.

The STM32CubeMonitor team.

This topic has been closed for replies.
Best answer by Richard.Chvr

Version 1.4.0 is available from now, it can be used instead.

1 reply

Richard.Chvr
Richard.ChvrBest answer
Technical Moderator
March 30, 2022

Version 1.4.0 is available from now, it can be used instead.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.