Accessing UCPD monitor via USB to UART bridge
Hello,
I would like to ask a question, if it is possible to access UCPD monitor via USB-UART bridge? I am following tutorial AN5418, with nucleo G0B1RE and SNK1M1 shield. Everything works fine when I use st-link, but when using uart bridge I dont see the board in board selection of UCPD and can log data only to UCPD trace...
I have found out, that one can make it to work when one desolderes SB16 and SB15 from st-link on nucleo and connects LPUART to TX and RX of JP6. But is it also possible to make it work with USB-UART bridge from another vendor?

Thanks,
Marosh