Skip to main content
Graduate II
September 20, 2025
Question

Difficulty to watch the variables disabled in cubemonitor

  • September 20, 2025
  • 2 replies
  • 363 views

Iam using cube monitor which is off course a very useful tool for debugging but only difficulty iam facing is when i disable the variables which i don't want to see or completely invisible, could you please bring in something so that it can be visible even if disabled. Ex image below

STuser2_0-1758363255074.png

If you see above image the disabled variables are completely invisible for me to make them enable again.

 

    This topic has been closed for replies.

    2 replies

    Technical Moderator
    September 25, 2025

    Hello @STuser2 

    You would like to have an option to hide/unhide variables from the graph upon clicking on their name, is that right?

    STuser2Author
    Graduate II
    September 25, 2025

    What i am trying to say is that even if i make variables as hidden, after some time i may want to watch the variables (hidden) again so it should be partially visible instead of completely hidden.