Skip to main content
Visitor II
February 16, 2021
Solved

Is it possible to distinguish between multiple debug probes?

  • February 16, 2021
  • 2 replies
  • 1337 views

Hello.

Firstly - thank you for a great tool.

My issue is that I am debugging several systems in parallell. The monitor is great for this. But I happends to have several ST-Link probes with serial numbers that ends with the same numbers. As I am adding more probes, it becomes impossible to tell them apart. The names all comes up with only the last digits of the serial number and no way to rename them. Am I missing something or will it be possible to have the complete serialnumber in the name?

Best regards

Hans Rosendahl

    This topic has been closed for replies.
    Best answer by stephane.legargeant

    Hello.

    I have done some check, and even if the tools displays only the last digit, it uses the full serial number internally. So you should be able to manage the probes properly.

    What you can do : test with the "blink led" (button with a bulb). You will see the led of STLINK blinking and you can identify which probe is where. Then the tool should work properly.

    I have not been able to test, as I don't have ST-LINK with the same ending digits. May be the clone have a strange numbering ?

    Best regards

    Stephane

    2 replies

    ST Employee
    February 16, 2021

    Hello

    It seems that tools use only the last digits to manage the probes. I can check with my colleagues if changing the number is possible. What type of probes are you using ?

    Stephane

    Graduate II
    February 16, 2021

    Bootleg...

    Does it use the UNIQUE ID of the STM32 doing the ST-LINKing?

    Super User
    February 16, 2021

    Yes it looks so. The unique digits are in the middle of the string, not the last ones.

    (solution is obvious)

    -- pa

    HRose.3Author
    Visitor II
    February 16, 2021

    Thank you for your quick answer.

    Currently I am using clone ST-LINK V2 probes. It makes sense if the tools only use the last digits, as the monitor actually connected to the wrong probe. Would there be any chance for making the tools use the whole serial number? Or - as you suggested - changing the serial number? It would be really powerfull to be able to monitor all mcu's in our system from one pc.

    Hans

    ST Employee
    February 17, 2021

    Hello.

    I have done some check, and even if the tools displays only the last digit, it uses the full serial number internally. So you should be able to manage the probes properly.

    What you can do : test with the "blink led" (button with a bulb). You will see the led of STLINK blinking and you can identify which probe is where. Then the tool should work properly.

    I have not been able to test, as I don't have ST-LINK with the same ending digits. May be the clone have a strange numbering ?

    Best regards

    Stephane