LPM01a enumaration fails when powered from USB host port.
Hi,
I purchased new LPM01a board for power consumption analysis. When I am powering it up with usb host port (JP3 -> usb) red led light up. I tried with different hosts (desktop and laptop) but that does not works. I am getting error "Get current range command failed" in STM32CubeMonitor-Power. From google I found out that pc current limit is upto 100mA only. However, in user manual of LPM01, it specified that 500mA is required for working otherwise red led will light up.
My first question is, if PC can be configared to deliver current upto 500mA, then how?
Alternatively, LPM01 can be also powered from external CN7 jumper with JP3 set to Ext.
In this regard, My 2nd question is:
In Ext power mode, data acquisition with STM32CubeMonitor-Power is still possible via usb port (CN5), or only the board display is available?