STM-Studio Import Variables fails
Hello, after selecting the .elf file I get hundred of messages of this type:
GDB Cmd [print /x & arm_cfft_sR_f32_len128.pTwiddle] failed
Error: Address of symbol "arm_cfft_sR_f32_len128" is unknown
and similar, all related to CMSIS.
After I ack all of these errors the import restarts with the same errors, only way out is by killing the program via process manager.
All OK when variable addresses taken from .map are inserted, big pain but OK.
What can be done?
I'm aware of STMCubeMonitor, tried it but it looks like it's a joke, or at least not what I need. I just need a scope and a table to read and write variables. AFAIK CubeMonitor does not even have vertical scale adjust, just to mention the first showstopper.
I'm shure that 99% of people share my needs.
BTW STMCubeMonitor could conveniently be replaced with a binding to Python or whatever, then everybody chooses his own gui, framework etc.