STM32CubeMonitor-1.5.0 is available
Hello
A new version 1.5.0 of STM32CubeMonitor is available on st.com.
You can download it on https://www.st.com/en/development-tools/stm32cubemonitor.html
Click on "Get latest" to download the version 1.5.0.
What are the changes in this version ?
The management of multiple probes has been improved to add a new acquisition mode. The changes performed in version 1.4.0 provided better performance with an increase of the CPU usage. However this level of CPU load is irrelevant for users performing low speed acquisition (i.e. 1Hz), so that a new “ECO MODE�? has been added to better address this case : if the acquisition speed is lower than 10Hz, then the new Eco mode is automatically activated to reduce the CPU load. If needed, the threshold can be changed in the setting.js file.
Node-RED® is updated to version 3 (V3.0.2) :
Node-RED® dashboard version updated to 3.1.73.
Update of serial-port node to 1.0.1
3 new dashboard nodes have been added to display specific information :
- 3D shows a picture with 3D orientation,
- radar shows dots on a circle,
- activity shows some “activity�? icons (walk, run,…)
There are also some fix for issues reported in the forum :
- Solved acquisition problem with multiple probes on Ubuntu 20.04
- Log to CSV variable name with dot character
- “Cannot secure Node-RED® on Ubuntu®�? is fixed
Do not hesitate to create new posts if you have any question.
The STM32CubeMonitor team.