Skip to main content
ST Employee
November 19, 2020
Solved

STM32CubeMonitor-RF V2.6.0 released

  • November 19, 2020
  • 1 reply
  • 792 views

New version 2.6.0 is released.

New features :

Some 802.15.4 RF tests are added to make certification tests easier :

  • In the transmitter test,it is possible to send MAC frames . The frame can be defined by the user.
  • In the receiver test, the LQI, ED, and CCA tests are available and the PER test shows the decoded frames.

Fixed issues :

  • Fixes the blank popup message displayed when the script detects an error,
  • Includes workaround to prevent some freeze observed on a serial port with MacOS.
  • Disables the navigation link when the 802.15.4 receiver test is in progress,
  • Updates ST logo and colors,
  • Disables the start button as soon as the channel list is inconsistent in 802.15.4 PER multi-channel test,

Restrictions :

  • In the OTA Updater panel, the Image base address bytes are inverted. To flash at address 0xAABBCC, user must set 0xCCBBAA. The default value 0x7000 is working because it is equivalent to 0x007000 and inversion has no effect.
    This topic has been closed for replies.
    Best answer by stephane.legargeant

    This thread has been closed to avoid multiple conversations happening on the same thread. Please create a new thread if you wish to ask questions or discuss this update.

    1 reply

    ST Employee
    November 24, 2020

    This thread has been closed to avoid multiple conversations happening on the same thread. Please create a new thread if you wish to ask questions or discuss this update.