STM32CubeMonitor - Trigger SW Reset
Hello,
I would like to trigger a STM32 device reset from inside STM32CubeMonitor.
I'm developing an application using STM32CubeIDE and STM32CubeMonitor. Duringe measuring of my variables via STM32CubeMonitor it is possible that my device gets into a reduced function safe state (on purpose). Then it would be very helpful to trigger a device reset via a button like I'm able to do during debugging in STM32CubeIDE.
I understand currently only the topics: Read, Start and Stop are available for a probe-node. Is it possible to trigger a reset via additional (maybe undocumented) options or is this feature planned in a future release?
If not is there a workaround available? I tried to connect to the GDB server opened by the probe-node after starting the acquisition but wasn't successful. As far as a saw it, the server is always opend on a different port?!.
Thank you
Best regards
Martin