Wireless Long Range RF Test - STM32CubeMonitor - two boards NUCLEO-WL55JC - how to make tests with t
Hallo,
I have two NUCLEO-WL55JC boards with dedicated FW (LoRaWAN\LoRaWAN_AT_Slave) for making some tests with STM32CubeMonitor. Everything works fine, tests are possible without problems, but these two boards are connected to the same computer. That's why I cannot say, that I am doing some long range tests - rather very short range tests... The range is limited by the length of two USB cables (between each Nucleo and USB port).
So - the question is: Is there possible, to make real long range test with two boards? IIf yes, how to do it? Do I need two persons with two computers (each board connected to each computer), calling by the phone to each other and starting the dedicated tests - what should be the procedure? One starts RX Test and the other Tx Test (for example for RF Test Tone(CW))?

Or maybe do I need only one PC and one board connected to it, and the second Nucleo will work in automated way?
Regards
Paul