Skip to main content
Technical Moderator
May 4, 2026
Question

Test STM-UAT4

  • May 4, 2026
  • 2 replies
  • 34 views

Hello,

This is for test 

  1. BOOT1 jumper is set to HIGH for development (DEV boot mode)
  2. I have a simple LED blink application built with GPIO configured in the FSBL context
  3. The code runs as expected in DEV mode (debug mode of STM32CubeIDE)
  4. I then flashed the signed binary in external memory using STM32CubeProgrammer and External Memory loader for Nucleo-N6 board at address 0x70000000. 
  5. Then, I switched BOOT-1 jumper to LOW and reset the board. The code runs as expected from external memory
  6.  

Edit: new test 😀

 

2 replies

Imen.DAuthor
Technical Moderator
May 4, 2026

thanks for this post

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
Amel NASRI
Technical Moderator
May 7, 2026

subscribed to the forum

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.