auto start SWV
Hi,
the Serial wire viewer (SWV) has a command-line option.
This only launch the viewer and the user has to press R to start.
Is it possible to directly start the SWV?
Or is there a shell trick for this?
- Thomas
*********************************************
Manual
STM32_Programmer_CLI.exe -c port=swd -swv freq=32 portnumber=0
C:\Users\ST\swvLog\example.log
Serial wire viewer (SWV) command
-SWV
Description: This command allows the user to access the serial wire viewer console mode,
which displays the printf data sent from the target through SWO.
In this mode (see Figure 105) the user can start and stop the reception of the SWO data by pressing, respectively, the “R�? and “S�? buttons on the keyboard. T