Skip to main content
jefflongo
Associate III
January 11, 2020
Solved

BOOT0/NRST control with DTR/RTS

  • January 11, 2020
  • 7 replies
  • 8428 views

Is it possible to use the DTR/RTS pins of a UART bridge (such as FT232RL) to automate entering the bootloader in system memory for flashing firmware using STM32CubeProgrammer? Has anybody achieved this?

This topic has been closed for replies.
Best answer by jefflongo

As it turns out, I discovered DTR (if inverted) can be used for BOOT0, and RTS for NRST. This didn't work properly in the GUI version, but in the command line interface it did in fact work.

7 replies

jefflongo
jefflongoAuthorBest answer
Associate III
January 16, 2020

As it turns out, I discovered DTR (if inverted) can be used for BOOT0, and RTS for NRST. This didn't work properly in the GUI version, but in the command line interface it did in fact work.

waclawek.jan
Super User
January 16, 2020

Thanks for the information.

This really ought to go into the documentation ( @Imen DAHMEN​ can you please have a look at this); and also ought to work in the GUI.

JW

Technical Moderator
January 16, 2020

Hello,

I will raise this issue internally for check. We will come back to you soon with update.

Best Regards,

Imen

"When your question is answered, please close this topic by clicking ""Accept as Solution"".ThanksImen"
TVan .2
Associate II
March 29, 2020

@Imen DAHMEN​ any answer yet how to do this and with what tool? So auto reset and auto bootloader with dtr and rts?

Pavel A.
Super User
March 29, 2020

For example, the H750 board from this thread has USB to RS232 adapter wired to NRST and BOOT0.

The schema is posted in the thread.

-- pa

TVan .2
Associate II
March 30, 2020

Dear

This is DTR and DTS, my FT234XD doesn't have those. Only RTS and DTR.

Does this method work without any special software?

Greetings

Thomas Van Aken

jefflongo
jefflongoAuthor
Associate III
April 3, 2020

I was able to find a solution by writing a program which uses the FT232R GPIO to control NRST and BOOT0, calling STM32CubeProgrammerCLI. Pretty good software independent solution to me.​

TV_it
Associate II
November 26, 2021

I know this is an old thread, but could somebody tell me if this works now in STM32CubeProgrammer? Or if the FT232R GPIO control program is available somewhere?

jefflongo
jefflongoAuthor
Associate III
November 26, 2021

Hi,

Not sure if this works in STM32CubeProgrammer yet, but I was able to come up with a workaround, see here: https://github.com/jefflongo/stm32handsfree

TV_it
Associate II
November 27, 2021

Does this work under windows too?