Can external loader running on an STM32F030C8 be run from flash, or must external loaders always run from RAM
I am using an STM32f030C8 with External Flash (W25W128) Via SPI, and want to program the extern flash with sound data using STMcubeprogrammer.
I found an excellent article (https://community.st.com/s/article/how-to-add-your-spi-flash-into-the-stm32cubeprogrammer-external-loader-part1) that used a RAM based approach.
My question is can external loaders be a FLASH based program, and will STMcubeprogrammer load the external loader to allow programming of the extern Flash and then after that load the CPU flash with the real application code ?