Can I install STM32CubeProgrammer on my linux machine
Hello,
My Linux specs:
- Linux lime2 3.4.104-00136-gd47d367
- armv7l GNU/Linux
SetupSTM32CubeProgrammer.linux file's information:
- ELF 32-bit LSB executable
- Intel 80386
- version 1 (GNU/Linux)
- for GNU/Linux 2.6.24
- not stripped
When I try to install, error shows up saying that installation couldn't create folder /bin/ and temporary file "libstp11_SAM.so.conf".
When I manually add mentioned file and folder, installation finishes but I cannot run "STM32CubeProgrammer.desktop" file which is created on my desktop.
So, my question is whether I can install CubeProgrammer on my machine based on given specifications?
Thanks in advance,
A.C.