Skip to main content
PGorb.1
Visitor II
April 29, 2020
Question

Can't close app, if connection was failed.

  • April 29, 2020
  • 12 replies
  • 2274 views

Hello, i found next problem. If open app, and try connect to board with unsuccessful result, than app can't be closed any method, other than via task manager. In other case, app close via stantard button. This bug not disapering, if, for example, first try was failed, but few try later was successful. OS Windows 10 x64 (with last update at time of writing this topic). Tested chips: STM32L053 (custom board), STM32F031(NUCLEO-F031K6) .

This topic has been closed for replies.

12 replies

Nesrine.JLASSI
Visitor II
October 30, 2020

Hi @PGorb.1​ 

Please try with the last CubeProgrammer version (2.5.0) then tell me if it solve the issue.

Best regards,

Nesrine

Radosław
Associate II
November 2, 2020

Same problem also with 2.5.0. despribed earlier on this forum.

Nesrine.JLASSI
Visitor II
November 3, 2020

Hello @Rados?aw​ 

Tested the same scenario without getting issue. Please try to upgrade Firmware then tell me if the issue still exist.

0693W000005A9UKQA0.pngBest regards,

Nesrine

Radosław
Associate II
November 3, 2020
PS. Tested on new computer with win 10 pro, also 2 colleagues have same effect.
Radosław
Associate II
November 3, 2020

I use latest firmware.

I notice something else, config.properties file is empty

Nesrine.JLASSI
Visitor II
November 3, 2020

Could you please specify the board name.

Radosław
Associate II
November 3, 2020

Tested with STLINK V2-1 and V3. target must be unconnected

Radosław
Associate II
November 3, 2020

Next situation. Afted this blocked state, config.properties is empty, Next time with no stlink connected to PC i click connect, then config.properties include soome options. then ONLY ONES cube prog can be closed after failure conection to target.

Nesrine.JLASSI
Visitor II
November 4, 2020

Hi @Rados?aw​ 

Please check cables, a lot of people use ST-Link with success, so i think the problem is on your side.

0693W000005AHfLQAW.pngBest regards,

Nesrine

Radosław
Associate II
November 4, 2020

Please be serious. This is 3 or 4 topic with this problem, I desribe problem very detailed. Confirmed in few station, with many programmers.

THIS IS BUG.

Nesrine.JLASSI
Visitor II
November 4, 2020

Can you please specify you java version.