Cannot program with geniune ST Link/V2
Hi
I have been using Atollic for years , with the cheap stlink programmers from AliExpress. I havent had any issues, but just recently updated to STM32IDECube (V1.13.0) , and STM32CubeProgrammer (V2.14.0) . I purchased an original ST32Link-V2 , but unfortunately doesn't connect through either STM32CubeProgrammer or STM32IDECube. The cheap version works on STM32CubeProgrammer but not STM32IDECube , comes up "error No ST-Link Detected " (same error STM32IDECube for genuine). I am using pins:
SWDIO , SWCLK , GND . I also tried the Reset line on the genuine , but still error. On STM32IDECube I get "No ST-Link Detected.." on both the cheap and genuine one. On the STM32CubeProgrammer works as expected with the cheap one, with the genuine one I get error DEV_TARGET_HELD_UNDER_RESET if I attach the reset line, and no STM target found error without it. I have the RST line on the processor pulled up with external 10k, and BOOT0 pin pulled low with 10k. I got my hands on another genuine programmer and just the same, so know the new one works.
Regarding the ST-Link configuration on the STM32Programmer, I have tried all the possibilities without any luck.
Any help would be great,
Thanks
Scott