Skip to main content
kalvacherla.chandrashekhar
Associate III
October 13, 2020
Solved

Deadlock on STM32H745I-Disco board and it Throws error "No STM32 target Found" in STM32CubeProgrammer

  • October 13, 2020
  • 1 reply
  • 1446 views

Deadlock on STM32H745I-Disco board .

The STM32H745I-Disco board Throws error "No STM32 target Found" in STM32CubeProgrammer .

Can we recover this Board if the TAG connector is connected to SEGGER DEBUG Adapter

0693W000004JZZjQAO.png 

11:10:20 : STM32CubeProgrammer API v2.5.0

11:10:36 : Read File: C:\Users\180200_sgpcu\Documents\LOCAL\STM32H745I\STM32H745I\CM7\Debug\STM32H745I_CM7.bin

11:10:36 : Number of segments: 1

11:10:36 : segment[0]: address= 0x0, size= 0x313C

11:10:41 : ST-LINK SN : 0027003E3137510F39383538

11:10:41 : ST-LINK FW : V3J7M2

11:10:41 : Board : STM32H745I-DISCO

11:10:41 : Voltage : 3.27V

11:10:41 : No STM32 target found!

11:10:41 : ST-LINK SN : 0027003E3137510F39383538

11:10:41 : ST-LINK FW : V3J7M2

11:10:41 : Board : STM32H745I-DISCO

11:10:41 : Voltage : 3.27V

11:10:41 : Error: No STM32 target found!

11:14:10 : Error: No debug probe detected.

11:14:33 : ST-LINK SN : 0027003E3137510F39383538

11:14:33 : ST-LINK FW : V3J7M2

11:14:33 : Board : STM32H745I-DISCO

11:14:33 : Voltage : 3.26V

11:14:33 : No STM32 target found!

11:14:33 : ST-LINK SN : 0027003E3137510F39383538

11:14:33 : ST-LINK FW : V3J7M2

11:14:33 : Board : STM32H745I-DISCO

11:14:33 : Voltage : 3.27V

11:14:33 : Error: No STM32 target found!

11:41:12 : ST-LINK SN : 0027003E3137510F39383538

11:41:12 : ST-LINK FW : V3J7M2

11:41:12 : Board : STM32H745I-DISCO

11:41:12 : Voltage : 3.27V

11:41:13 : Error: No STM32 target found!

11:41:22 : ST-LINK SN : 0027003E3137510F39383538

11:41:22 : ST-LINK FW : V3J7M2

11:41:22 : Board : STM32H745I-DISCO

11:41:22 : Voltage : 3.27V

11:41:22 : Error: No STM32 target found!

11:41:27 : ST-LINK SN : 0027003E3137510F39383538

11:41:27 : ST-LINK FW : V3J7M2

11:41:27 : Board : STM32H745I-DISCO

11:41:27 : Voltage : 3.27V

11:41:27 : Error: No STM32 target found!

11:41:31 : ST-LINK SN : 0027003E3137510F39383538

11:41:31 : ST-LINK FW : V3J7M2

11:41:31 : Board : STM32H745I-DISCO

11:41:31 : Voltage : 3.27V

11:41:31 : Error: No STM32 target found!

11:41:48 : ST-LINK SN : 0027003E3137510F39383538

11:41:48 : ST-LINK FW : V3J7M2

11:41:48 : Board : STM32H745I-DISCO

11:41:48 : Voltage : 3.27V

11:41:48 : No STM32 target found!

11:41:48 : ST-LINK SN : 0027003E3137510F39383538

11:41:48 : ST-LINK FW : V3J7M2

11:41:48 : Board : STM32H745I-DISCO

11:41:48 : Voltage : 3.27V

11:41:48 : Error: No STM32 target found!

11:41:58 : ST-LINK SN : 0027003E3137510F39383538

11:41:58 : ST-LINK FW : V3J7M2

11:41:58 : Board : STM32H745I-DISCO

11:41:58 : Voltage : 3.27V

11:41:58 : Error: No STM32 target found!

11:42:00 : ST-LINK SN : 0027003E3137510F39383538

11:42:00 : ST-LINK FW : V3J7M2

11:42:00 : Board : STM32H745I-DISCO

11:42:00 : Voltage : 3.27V

11:42:00 : Error: No STM32 target found!

11:42:02 : ST-LINK SN : 0027003E3137510F39383538

11:42:02 : ST-LINK FW : V3J7M2

11:42:02 : Board : STM32H745I-DISCO

11:42:02 : Voltage : 3.27V

11:42:02 : Error: No STM32 target found!

This topic has been closed for replies.
Best answer by Tesla DeLorean

With BOOT0 pulled high, cycle the power several times until you can attach and erase the program in Flash.

Check the LDO/SMPS and VOS settings in your code carefully so they don't jam up the board in this fashion.​

1 reply

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
October 13, 2020

With BOOT0 pulled high, cycle the power several times until you can attach and erase the program in Flash.

Check the LDO/SMPS and VOS settings in your code carefully so they don't jam up the board in this fashion.​

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
kalvacherla.chandrashekhar
Associate III
October 15, 2020

Hi ,

Yes the STM32H7 was Bricked , I am able to now recover the board 10K resistance De-Soldered from R143 and Soldered on to R144 .( There should have been an Jumper provided or ,, the ST-LINK should have had GPIO method to recovered the board )

0693W000004Jt3OQAS.pngAfter Going through the user manual it is mentioned in an Caution: :sad_but_relieved_face: