Question
Did I brick my STM32F2?
Hi all -
I'm modifying some legacy code written for a WICED device that contains an STM32F2xx. The original programmer had a passage that reduces down to:
#define OB_RDP_Level_0 ((uint8_t)0xAA)
#define OB_RDP_Level_1 ((uint8_t)0x55)
FLASH_OB_Unlock();
FLASH_OB_RDPConfig( OB_RDP_Level_1 );
FLASH_OB_Launch();
FLASH_OB_Lock();
NVIC_SystemReset( );I have no idea where he got the value "55" but the upshot is I can't reset my OBs. When I try, I get this output from the programmer software:
15:15:33 : Option byte command : -ob RDP=170
15:15:33 : PROGRAMMING OPTION BYTES AREA ...
15:15:33 : Bank : 0x00
15:15:33 : Address : 0x40023c14
15:15:33 : Size : 12 Bytes
15:15:52 : UPLOADING OPTION BYTES DATA ...
15:15:52 : Bank : 0x00
15:15:52 : Address : 0x40023c14
15:15:52 : Size : 12 Bytes
15:15:52 : Error: Uploading Option Bytes bank: 0 failed
15:15:52 : Error: Reloading Option Bytes Data failed
15:15:52 : Time elapsed during option Bytes configuration: 00:00:18.761
15:15:52 : Error: Unable to get core ID
15:15:52 : Error: Unable to get core ID
15:15:52 : Warning: Connection to device 0x411 is lost
15:15:52 : Disconnected from device.So, my questions are:
- does anyone know what a value of "55" will do in this situation? (I guess what I'm really asking is, is it possible that it got interpreted as "CC"?)
- Any suggestions for un-bricking this? I've unplugged and disconnected everything a few times.
Thanks for any assistance...