Skip to main content
SegmentFault
Associate II
August 5, 2020
Question

Error: Could not find or load main class com.st.app.Main on Linux

  • August 5, 2020
  • 0 replies
  • 651 views

Hello,

I installed STM32CubeProgrammer on Ubuntu 18.04 and when I run it using the graphical interface the program does not start. If I start It using the command line I can see the following error

Error: Could not find or load main class com.st.app.Main

I was using Java 8. I tried to use java 11 using the following command

sudo update-alternatives --config java

And now I get the following error:

Error: Could not find or load main class com.st.app.Main
caused by: java.lang.NoClassDefFoundError: javafx/application/Application

Regarding the java versions that I used this is the output of java -version when java8 was selected

openjdk version "1.8.0_252"
OpenJDK Runtime Environment (build 1.8.0_252-8u252-b09-1~18.04-b09)
OpenJDK 64-Bit Server VM (build 25.252-b09, mixed mode)

and this is the output of java -version when java 11 was selected

openjdk version "11.0.8" 2020-07-14
OpenJDK Runtime Environment (build 11.0.8+10-post-Ubuntu-0ubuntu118.04.1)
OpenJDK 64-Bit Server VM (build 11.0.8+10-post-Ubuntu-0ubuntu118.04.1, mixed mode, sharing)

So, how can I run STM32CubeProgrammer from Linux?

This topic has been closed for replies.