Question
Error: failed to download Segment[0], Error: failed to download the File
Hi,
I'm trying to create a C# wrapper for STM32CubeProgrammer_API.dll.
In version 2.10, the downloadFile function worked perfectly within my C# wrapper. However, upon updating to version 2.15 of the STM32CubeProgrammer_API.dll, the function no longer operates as expected.
This is the output I receive when I try to use the function
Memory Programming ...
Opening and parsing file: data.hex
File : data.hex
Size : 3.76 KB
Address : 0x08000000
File segment @0x08000000 is not 255-bytes aligned. It will be aligned to @0x07FFFFF8
Download in Progress:
Size : 4080 Bytes
Address : 0x07FFFFF8
Buffer program...
w ap 0 @0x07FFFFF8 : 0x00000FF0 bytes, Data 0xFFFFFFFF...
Error: failed to download Segment[0]
Error: failed to download the File
Thanks