Error to connect to target STM32H747I-DISCO
I try to connect to target STM32H747I-DISCO but show this message:
08:58:19 : ST-LINK SN : 004800413137510D39383538
08:58:19 : ST-LINK FW : V3J3M2
08:58:19 : Voltage : 3.27V
08:58:19 : No STM32 target found!
08:58:20 : ST-LINK SN : 004800413137510D39383538
08:58:20 : ST-LINK FW : V3J3M2
08:58:20 : Voltage : 3.27V
08:58:20 : Error: No STM32 target found!
And the file in FAIL.TXT with:
The interface firmware FAILED to reset/halt the target MCU
how can I solve that?