Error "unable to connect to the target" while flashing to ST NUCLEO-H7A3ZI-Q board.
Hai, I am using ST NUCLEO-H7A3ZI-Q board and I am new it. It worked properly for first one or two times. But now I cant flash code into it, it say "unable to connect to the target". Then I tried STM32CubeProgrammer to connect it and ts connected in 'Power down' mode. Then I performed Full chip erase. After that the board worked properly.
But the problem arises again when I reconnected the board and I done the full chip erase again.
That is I need to run the full chip erase every time I power the board.
How can I resolve the problem?
Thank you.
Sachin