External Loader buffer size
Hello ST Community,
I’m developing a custom external loader for STM32CubeProgrammer where the STM32 acts as a bridge to program an external MCU (not external flash). The STM32 uses UART5 as a debug port and also as the communication interface to the external MCU.
In testing, I see CubeProgrammer calling Write() repeatedly with non‑sector‑aligned sizes and addresses that don’t start at sector boundaries. Sample output from my loader:
Starting... Address: 0x90000000 Size: 0x0003C700 Size is not sector aligned:0x0003C700 Address: 0x9003C700 Size: 0x0003C700 Size is not sector aligned:0x0003C700 Address is not start of sector:0x9003C700 ... Address: 0x901E3800 Size: 0x00018E00 Size is not sector aligned:0x00018E00 Address is not start of sector:0x901E3800 Address: 0x901FC600 Size: 0x00018E60 Size is not sector aligned:0x00018E60 Address is not start of sector:0x901FC600
This looks like CubeProgrammer is splitting the image into chunks (e.g., 0x3C700, then smaller fragments near the end) and incrementing the Address, but not guaranteeing sector alignment. I understand this is expected for external flash loaders (since the loader handles alignment/erase internally), but in my case the target is an external MCU.
The external MCU requires sector-aligned writes because:
- It erases flash by sector before writing.
- It writes data sequentially based on a sector index. If CubeProgrammer sends a chunk that overlaps or partially rewrites a sector, the flashing process will fail.
How can I enforce sector alignment in CubeProgrammer?
Is there a way to configure CubeProgrammer so that all Write() calls are sector-aligned (both Address and Size)?
int Init(void)
{
*(uint32_t *)0xE000EDF0 = 0xA05F0000; // enable interrupts in debug
SystemInit();
SCB->VTOR = 0x20000000 | 0x200;
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
// For debug output
__HAL_RCC_UART5_FORCE_RESET();
__HAL_RCC_UART5_RELEASE_RESET();
MX_UART5_Init();
printf("Starting...\n");
/*
* Initialization function
*
*/
return LOADER_OK;
}
int Write(uint32_t Address, uint32_t Size, uint8_t *buffer)
{
printf("Address: 0x%08lX\n", Address);
printf("Size: 0x%08lX\n", Size);
// For external MCU programming, sector alignment required.
// Check that the size is sector aligned
if (Size % MEMORY_SECTOR_SIZE)
{
printf("Size is not sector aligned:0x%08lX\n", Size);
// return LOADER_FAIL;
}
// Check that the address is the start of a sector
if (Address % MEMORY_SECTOR_SIZE)
{
printf("Address is not start of sector:0x%08lX\n", Address);
// return LOADER_FAIL;
}
// Forward 'buffer' as-is to external MCU.
/*
* writing code
*/
return LOADER_OK;
}