Failed to erase memory (STM32F746G)
I am trying to upload a program to the board but i keep getting this error
Error: failed to erase memory
Read/Write protection is disabled and firmware is up to date (V2J33M25)
This is what i get in the LOG
13:49:39:117 : Memory Programming ...
13:49:39:117 : Opening and parsing file: ETH_FINAL.elf
13:49:39:139 : File : ETH_FINAL.elf
13:49:39:139 : Size : 12184 Bytes
13:49:39:139 : Address : 0x08000000
13:49:39:139 : Erasing Segment <0> Address <0x08000000> Size <12184>Bytes
13:49:39:139 : Erasing memory corresponding to segment 0:
13:49:39:139 : Memory erase...
13:49:39:139 : reset ap 0
13:49:39:139 : run ap 0
13:49:39:140 : halt ap 0 Status = 0
13:49:39:140 : w ap 0 reg 15 (0x20000000)
13:49:39:140 : w ap 0 reg 17 (0x20000500)
13:49:39:140 : w ap 0 reg 16 (0x01000000)
13:49:39:140 : w ap 0 @0x20000D80 0x00000200 bytes
13:49:39:140 : w ap 0 @0x20000000 0x00000004 bytes
13:49:39:223 : w ap 0 @0x20000004 0x00000954 bytes
13:49:39:223 : Erasing internal memory sector 0
13:49:39:223 : Init flashloader...
13:49:39:223 : halt ap 0
13:49:39:223 : w ap 0 reg 0 0x00000001
13:49:39:223 : w ap 0 reg 1 0x00000000
13:49:39:223 : w ap 0 reg 2 0x00000000
13:49:39:223 : w ap 0 reg 3 0x00000000
13:49:39:223 : w ap 0 reg 4 0x00000000
13:49:39:223 : w ap 0 reg 5 0x00000000
13:49:39:223 : w ap 0 reg 6 0x00000000
13:49:39:223 : w ap 0 reg 7 0x00000000
13:49:39:223 : w ap 0 reg 8 0x00000000
13:49:39:223 : w ap 0 reg 9 0x00000000
13:49:39:223 : w ap 0 reg 10 0x00000000
13:49:39:223 : w ap 0 reg 11 0x00000000
13:49:39:223 : w ap 0 reg 12 0x00000000
13:49:39:224 : w ap 0 reg 13 0x00000000
13:49:39:224 : w ap 0 reg 14 0x20000001
13:49:39:224 : w ap 0 reg 15 0x20000005
13:49:39:224 : w ap 0 reg 16 0x01000000
13:49:39:224 : w ap 0 reg 17 0x20000D54
13:49:39:225 : w ap 0 reg 18 0x00000000
13:49:39:225 : run ap 0
13:49:44:004 : halt ap 0
13:49:44:004 : Init function fail with timeout
13:49:44:023 : r ap 0 reg 16 0x01000003
13:49:44:023 : Loader sector erase...
13:49:44:023 : Error: failed to erase memory
13:49:44:032 : Error: failed to erase memory