Flash memory is always erased when I connect STM32CubeProgrammer to STM32H7B3i-dk board
Hi,
Not sure what I am doing wrong but when I program my STM32H7B3I-DK board with STM32CubeProgrammer, all seems fine, the application start to run and everything is okay.
The problem occurs when I click the Disconnect button and later then try to Connect at this point what everything I have programmed in the flash memory of device gets erased.
I am running the Secure Boot Secure Firmware Update (SBSFU) example program. Below is an image of my "Option Bytes" I can't see any of the flag to cause this behavior.