Skip to main content
STE_Michael
Associate
November 28, 2023
Solved

Generate srec file with option bytes configuration in offline mode?

  • November 28, 2023
  • 1 reply
  • 1521 views

Hello,

how can I generate a srec file with option bytes configuration in offline mode?
No St-Link and no hardware is connected!

STVP is an old tool which can do this simple things.

But it does not support all the microcontroller types (stm32Gxx).

Thank you for updating the version 2.15 to 3.0 ;)

 

 

 

 

 

This topic has been closed for replies.
Best answer by Maryem

Hello @STE_Michael,

Without connecting a device, it is not possible to read or write option bytes using STM32CubeProgrammer, as offline mode is currently unsupported. This means that generating the srec file with option bytes is also not possible. An internal ticket has already been submitted to the development team regarding your request.

Internal ticket number: 146447 (This is an internal tracking number and is not accessible or usable by customers).
I'll keep you posted.


Maryem.

1 reply

Maryem
MaryemBest answer
Technical Moderator
November 28, 2023

Hello @STE_Michael,

Without connecting a device, it is not possible to read or write option bytes using STM32CubeProgrammer, as offline mode is currently unsupported. This means that generating the srec file with option bytes is also not possible. An internal ticket has already been submitted to the development team regarding your request.

Internal ticket number: 146447 (This is an internal tracking number and is not accessible or usable by customers).
I'll keep you posted.


Maryem.