Skip to main content
Yoichi Shinoda
Senior
February 9, 2020
Question

H7A3ZI returns incorrect DFU memory descriptor?

  • February 9, 2020
  • 3 replies
  • 947 views

It seems that H7A3ZI on Nucleo-H7A3ZI-Q is returning incorrect memory descriptor:

@Internal Flash /0x08000000/256*02Kg,@Option Bytes /0x1FF8000/01*128 e,@OTP Memory /0x1FF7000/01*1024 e

Which tells there are only 256 of 2K (512KB); it should have 2MB, right?

STM32CubeProgrammer is probably also complaining:

17:47:13:733 : received memory address is wrong or unsupported
17:47:13:734 : Status: errVENDOR, State: dfuERROR
17:47:13:734 : failed to read the requested memory content
17:47:13:734 : Could not read flash size at address 0x8fff80c

Any info on this?

This topic has been closed for replies.

3 replies

Yoichi Shinoda
Senior
February 12, 2020

Since H7A3 is capable of erasing at 8KB sector unit, I believe the correct descriptor for the internal flash would be

@Internal Flash /0x08000000/256*08Kg

instead of

@Internal Flash /0x08000000/256*02Kg

Yoichi Shinoda
Senior
February 18, 2020

FYI, silicon revision for the problematic chip is 'Z'.

Yoichi Shinoda
Senior
May 12, 2020

Another piece of information regarding DFU device descriptor for H7A.

There is an example project for H7A which implements standalone DFU in STM32Cube_FW_H7_V1.6.0, and the descriptor used is partially correct as it uses 8KB page instead of 2KB page from the embedded boot loader.

STM32Cube_FW_H7_V1.6.0/Projects/NUCLEO-H7A3ZI-Q/Applications/USB_Device/DFU_Standalone/USB_Device/App/usbd_dfu_flash.c: line 66

#define FLASH_DESC_STR "@Internal Flash /0x08000000/6*8Ka,122*8Kg"

I'm wondering if newer silicon revision fixes this problem.

Tesla DeLorean
Guru
May 12, 2020

>>I'm wondering if newer silicon revision fixes this problem.

I seem to recall the system memory being flash/otp so flaws in the loader would be addressed in programming/testing phase.

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..