Skip to main content
Gdönm.1
Associate
March 21, 2021
Solved

how can i pass step 7 while setup stm32 cube programmer

  • March 21, 2021
  • 9 replies
  • 4010 views

when i create this program everything is ok until step7. however i cant pass step 7

and window is below.0693W000008xUekQAE.png

This topic has been closed for replies.
Best answer by Houda GHABRI

Hi @Gokhan dönmez​ ,

To be honest it is the first time we see this behavior :) .

Just to be sure, can you confirm if you install the STM32CubeProgrammer tool using these steps:

  • Download STM32CubeProg-Win-64bits zip package (64bits because you are using win10 (64 bits))
  • Extract the zip package
  • Execute SetupSTM32CubeProgrammer-vx.y.z.exe (Run as admin ) ,which guides you through the installation process.

Houda

9 replies

Houda GHABRI
ST Employee
March 22, 2021

Hi Gdönm.1

Can you please tell more informations :

  • which CubeProgrammer version you are using?
  • Which OS you are you using, is it on Windows?

Houda

Gdönm.1
Gdönm.1Author
Associate
March 22, 2021

Hİ Houda Ghabri,

Sure ,

i m using version 2.7.0 CubeProgrammer

I m using win10 (64 bits).

Thanks for answer.

Gokhan.

Houda GHABRI
ST Employee
March 23, 2021

Hi @Gokhan dönmez​ ,

Can you please try to install CubeProgrammer with admin rights in new folder and tell me if it is OK?

Houda

Gdönm.1
Gdönm.1Author
Associate
March 23, 2021

Hi Houda Ghabri

I tried to install Cubeprogrammer with admin rights in new folder now but i don't install it.

Gokhan

Houda GHABRI
Houda GHABRIBest answer
ST Employee
March 26, 2021

Hi @Gokhan dönmez​ ,

To be honest it is the first time we see this behavior :) .

Just to be sure, can you confirm if you install the STM32CubeProgrammer tool using these steps:

  • Download STM32CubeProg-Win-64bits zip package (64bits because you are using win10 (64 bits))
  • Extract the zip package
  • Execute SetupSTM32CubeProgrammer-vx.y.z.exe (Run as admin ) ,which guides you through the installation process.

Houda

Houda GHABRI
ST Employee
April 1, 2021

Hi Gdönm.1,

I'm coming back to see if it works for you since my last answer.

I hope so :)

Houda

AI1
Associate
April 21, 2022

Hello,

I am having the same problem , I tried above steps and nothing changed.In step7 I can't pass this step.

If you have found the reason, could you please share it!

Thanks .

0693W00000LyaBxQAJ.png

KUçan.1
Visitor II
May 5, 2022

Hi I have the same issue, I tried to load it to a different folder with admin rights as you said but it didn't work. Have anybody solved it?

Pavel A.
Super User
May 5, 2022

What if you do NOT enable creating any shortcuts on a previous step?

KUçan.1
Visitor II
May 5, 2022

enabling shortcuts is in step 7 which is shown empty as others have posted. In step 6 the files and drivers are downloaded after the download, I press next and an empty page with only one option "quit" is shown (It is same as the others have posted the screen shot of).

Bkork.1
Visitor II
August 8, 2022

0693W00000QNEUUQA5.png 

operating system: windows 10 pro x64

I'm trying to install cubeprogrammer v2.11.0

Can't get past the screen above.

I formatted the computer and it still didn't work.

I tried all of the above answers and it still didn't work.

(the answers above don't work.)

YToks.1
Visitor II
November 20, 2022

I had the same issue as Gdönm.1 and i was surfing at the stmcubeprogrammer files and i've found this so i clicked and it worked ! Maybe this could work for you too.0693W00000WIw9AQAT.jpg

Explorer
March 28, 2024

Thank you very much, this is the solution, I registered on that forum to say this :D