How do I regain ST-Link connectivity with Nucleo-H745ZI-Q with BOOT_CM7 = 0 and BOOT_CM4 = 1
While fiddling with H745 board to investigate how dual core works, after modifying option byte to BOOT_CM7 = 0 and BOOT_CM4, STM32CubeProgrammer (nor STLINK-gdbserver) refuses to connect to the board with "Error: No STM32 target found". The ST-Link itself is okay. Here is a log from the programmer.
22:31:39 : ST-LINK SN : 002F003D3137510E39383538
22:31:39 : ST-LINK FW : V3J5M2
22:31:39 : Voltage : 3.30V
22:31:39 : No STM32 target found!
22:31:39 : ST-LINK SN : 002F003D3137510E39383538
22:31:39 : ST-LINK FW : V3J5M2
22:31:39 : Voltage : 3.30V
22:31:39 : Error: No STM32 target found!How do I regain access to the board?