Skip to main content
AI1
Associate
April 27, 2022
Question

How to disable Core M4 Boot? Is it possible to work on debug mode with one core without disable one of them ?

  • April 27, 2022
  • 2 replies
  • 2073 views

I cannot install properly stm32cubeprogrammer after installation step 6 it is not installing even if I use an individual laptop. So I could not be able to over the stm32cubeprogrammer. I didn't find a topic about installation problems for stm32cubeprogrammer especially.I need help for installation if it is the one solution to disable core M4 boot !

Any help would be helpful.Thanks in advance.

This topic has been closed for replies.

2 replies

TDK
Super User
April 27, 2022

This error gets reported occasionally, I'm not aware of a good solution. What OS are you using?

M4 core can be disabled by unchecking BOOT_CM4 in the option bytes.

AI1
AI1Author
Associate
April 28, 2022

Thanks for your time and ans.

I am using Windows 11 - 64 bit OS - Version 21H2 .

To be able to do that I need to achieve the installation problem asap . It would be good that know the how issue solved .

As far as I know , there is only way to boot disable cores over the stm32cubeprogrammer with option bytes like below figure.

Are there any different solution to do that ?

Thanks.

0693W00000LzHrhQAF.png