Skip to main content
smade
Visitor II
September 2, 2019
Question

I have a st32f407vet6 card that I was connected to with the st link utility, but then when I connected with the st cube programmer, the card was blocked. Please help how to unblock

  • September 2, 2019
  • 2 replies
  • 890 views

..

This topic has been closed for replies.

2 replies

Imen Ezzine
ST Employee
September 10, 2020

Hi smade ,

It would help if you can provide more information. I don't believe a simple connection of the board to the cube programmer IDE could harm or block it, unless you did modify some parameters especially the option bytes...Is this the case here? and if so could you detail the steps you followed in order to help you unblock the board?

Also it will be good if you can precise what kind of message error you receive when connecting the board ( like is target not detected or halted etc...)

-Imen

BBOUR.1
Visitor II
September 13, 2020

Hi Imen,

I use ST_Link V2 for programming an debuging. So you can use STMCubeIDE or IAR to communicate with the VET6.

In configuration select ST-Link V2, SWD mode and not JTAG mode.

Hope this will help.

Benyoucef

Tesla DeLorean
Guru
September 13, 2020

Blocked? Bricked?

Do you connect NRST pin? Needed for "Connect Under Reset"

Can you connect with BOOT0 pulled HIGH?

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..