Skip to main content
rohitsam
Explorer
October 12, 2020
Question

Im unable to programe Stm32f411-disco board via USB with internal DFU on Cube programmer?

  • October 12, 2020
  • 0 replies
  • 547 views

The datasheet of stm32f411 says it supports USB DFU bootloader, but Im unable to programe Stm32f411-disco board via USB with internal DFU on Cube programmer, I have connected the boot0 to vdd and using the USB connected to PA11\PA12 for DFU.

Is there any specific hardware change that I have have this working?

Thank you.

This topic has been closed for replies.