Skip to main content
MDeva.1
Associate III
August 4, 2022
Question

In cubeprogrammer unbale to add start address

  • August 4, 2022
  • 3 replies
  • 2188 views

Hello,

I am working on NUCLEO-H7 board . Its dual core CM7 and CM4. When I Erase the full flash then I click into erase and programming option but I unable to add start address . The core M7 is get programming , but in Core M4 i unable to do programming because in start address block I unable to write . i am using latest version of cubeprogrammer.0693W00000QMvVYQA1.png

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
August 4, 2022

Use a .BIN file, not a .ELF

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
MDeva.1
MDeva.1Author
Associate III
August 4, 2022

I am working on STM32CUBEIDE. In which folder I get the .bin file

Tesla DeLorean
Guru
August 4, 2022

Don't know, not my tools.

I'd imagine in similar place to .ELF if you've checked a "create .BIN" option, or you run objcopy

Other question would be why the .ELF doesn't work or infer the correct address, as it's an object file

Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
MDeva.1
MDeva.1Author
Associate III
August 4, 2022

0693W00000QMx2xQAD.png

Mike_ST
Technical Moderator
August 4, 2022

Hello,

there are options to create bin and hex, please check the following picture:0693W00000QMx3WQAT.pngThey should be created in the same directory as the .elf file.