Issues with GDB Server...Need help!!
I have an STLINK-V3SET connected to a Seeed Lora-E5. I also have a Nucleo L476 developement board with on-board STLINK. On the Seeed board I am able to connect STM32CubeProgrammer and have loaded a file. I cannot connect however STM32CubeIDE as I get an immediate failure to connect due to GDB server ....On the Nucleo I have successfully connected the STM Utility and downloaded a file but once again I cannot connect STM32CubeIDE. I downloaded all three of these apps today so they are the latest....CubeIDE is 1.10.0. The IDE was working just fine as I have flashed Nucleol476 and NucleoWB boards but somehow I have corrupted it's ability to use the GDB server. I deleted the debug and .launch but to no avail....Please help here as I no longer have the ability to use the IDE ?????
UPDATE:
removed 1.10.0 IDE and went back to 1.9.0....
Below is the message received as I tried to load the application and run it on a NucleoL476....it got farther than it has but still some sort of issue????
Further attempts to run the debugger yields immediate:
If I go to this location the .exe file does NOT exists....wth????? instead I see an ST-LINK_gdbserver.bat file which contains the following: (only god knows where the K drive is)
cmd /K "ST-LINK_gdbserver.exe -c config.txt || echo GDB server exited"