Solved
Output log showing HWrst mode while it's connected over DFU mode
- March 19, 2025
- 1 reply
- 568 views
I am building my own programmer app using the API provided with the CubeProgrammer program. If I follow the way I have to connect my board over DFU mode as in the USB_Example.cpp, this is the output:
STM32CubeProgrammer API v2.18.0 | Windows-64Bits
+++ USB Bootloader Example +++
------------- USB DFU List --------------
USB Port 0
USB index : USB1
USB SN : 3768346A3430
DFU version : 0x11A
-----------------------------------------
USB speed : Full Speed (12MBit/s)
Manuf. ID : STMicroelectronics
Product ID : STM32 DownLoad Firmware Update
SN : 3768346A3430
DFU protocol: 1.1
Board : --
IAP
--- Device Connected ---
while in the CubeProgrammer app, doing, I guess, exactly the same, this is the output:

It's showing the same output but with an extra line:
08:53:09: UR connection mode is defined with the HWrst reset mode
If I search in the cli documentation it says that this is reserved only for JTAG/SWD debug:
-hardRst : Hardware reset
Available only with JTAG/SWD debug port
So why I am getting this line if I am connecting over DFU? and why is that line not showing in the output of the USB_example.cpp code?
Thanks
Rafa