Protecting IP while Flashing with STM32_Programmer_CLI - how?
Hi all,
Please let me know if this post belongs into the STM32 Security forum.
I'm developing a Windows GUI for flashing STM32H5 with my IP Software. The user of this GUI (customer) and the PC it's running on should NEVER be able to get a hold of the STM32 Software (.bin).
Caling STM32_Programmer_CLI from my GUI App (with -d or -w), it is only possible to provide the binary as a file.
I haven't tried using -w32, but I assume it will be rather slow for a ~megabyte-sized binary.
What I would love to do, is pipe the data into STM32_Programmer_CLI, but I don't think this is possible yet.
What is the best approach for hiding the binary and obk from theft, other than "securing by obscuring"?
Goal is to prevent the customer from flashing other MCUs without using my GUI (which contacts the license server).
Also, after Provisioning/Closing the device, the GUI would need to perform regression in order to reflash it, which again, could expose the password because the CLI only takes it as a file input...
Thanks in advance and best regards,
Stefan