Secure Firmware Install over USB on STM32H743
Is it possible to securely install firmware over USB on the STM32H743? I am getting the error below when trying to download my SFI file. MCU has been powered up with BOOT_0 pin high. STM32CubeProgrammer finds and connects correctly to chip.
11:03:34 : Starting Firmware Install operation...
11:03:34 : Activating security...
11:03:34 : Time elapsed during option Bytes configuration: 00:00:00.145
11:03:34 : Error: Activating security Failure
11:03:34 : OPTION BYTES BANK: 0
11:03:34 : Read Out Protection:
11:03:34 : RDP : 0xAA (Level 0, no protection)
11:03:34 : BOR Level:
11:03:34 : BOR_LEV : 0x0 (reset level is set to VBOR0)
11:03:34 : User Configuration:
11:03:34 : IWDG1_SW : 0x1 (Independent watchdog is controlled by software)
11:03:34 : IWDG2_SW : 0x1 (Independent watchdog is controlled by software)
11:03:34 : NRST_STOP_D1 : 0x1 (STOP mode on Domain 1 is entering without reset)
11:03:34 : NRST_STBY_D1 : 0x1 (STANDBY mode on Domain 1 is entering without reset)
11:03:34 : FZ_IWDG_STOP : 0x1 (Independent watchdog is running in STOP mode)
11:03:34 : FZ_IWDG_SDBY : 0x1 (Independent watchdog is running in STANDBY mode)
11:03:34 : SECURITY : 0x0 (Security feature disabled)
11:03:34 : BCM4 : 0x1 (CM4 boot enabled)
11:03:34 : BCM7 : 0x1 (CM7 boot enabled)
11:03:34 : NRST_STOP_D2 : 0x1 (STOP mode on Domain 2 is entering without reset)
11:03:34 : NRST_STBY_D2 : 0x1 (STANDBY mode on Domain 2 is entering without reset)
11:03:34 : SWAP_BANK : 0x0 (after boot loading, no swap for user sectors)
11:03:34 : IO_HSLV : 0x0 (Product working in the full voltage range, I/O speed optimization at low-voltage disabled)
11:03:34 : Boot address Option Bytes:
11:03:34 : BOOT_CM7_ADD0: 0x800 (0x8000000)
11:03:34 : BOOT_CM7_ADD1: 0x1FF0 (0x1FF00000)
11:03:34 : BOOT_CM4_ADD0: 0x810 (0x8100000)
11:03:34 : BOOT_CM4_ADD1: 0x1000 (0x10000000)
11:03:34 : PCROP Protection:
11:03:34 : PROT_AREA_START1: 0xFF (0x800FF00)
11:03:34 : PROT_AREA_END1: 0x0 (0x80000FF)
11:03:34 : DMEP1 : 0x1 (Flash Bank 1 PCROP zone is erased when RDP level regression (change from level 1 to 0) occurs)
11:03:34 : PROT_AREA_START2: 0xFF (0x810FF00)
11:03:34 : PROT_AREA_END2: 0x0 (0x81000FF)
11:03:34 : DMEP2 : 0x1 (Flash Bank 2 PCROP zone is erased when RDP level regression (change from level 1 to 0) occurs)
11:03:34 : Secure Protection:
11:03:34 : SEC_AREA_START1: 0xFF (0x800FF00)
11:03:34 : SEC_AREA_END1: 0x0 (0x80000FF)
11:03:34 : DMES1 : 0x0 (Flash Bank 1 secure area is kept when RDP level regression (change from level 1 to 0) occurs)
11:03:34 : SEC_AREA_START2: 0xFF (0x810FF00)
11:03:34 : SEC_AREA_END2: 0x0 (0x81000FF)
11:03:34 : DMES2 : 0x0 (Flash Bank 2 secure area is kept when RDP level regression (change from level 1 to 0) occurs)
11:03:34 : DTCM RAM Protection:
11:03:34 : ST_RAM_SIZE : 0x0 (2 KB)
11:03:34 : Write Protection:
11:03:34 : nWRP0 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP1 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP2 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP3 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP4 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP5 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP6 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP7 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP8 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP9 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP10 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP11 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP12 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP13 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP14 : 0x1 (Write protection not active on this sector)
11:03:34 : nWRP15 : 0x1 (Write protection not active on this sector)
11:03:34 : Error: failed to activate security!