Skip to main content
Associate
May 12, 2025
Question

sendOptionBytesCmd() function doest not work for my STM32G431CBY3TR

  • May 12, 2025
  • 4 replies
  • 515 views

Hello everyone,

I am currently writing a GUI application with QT. The STM32CubeProgrammer API is integrated in the project. So far I was able to flash FW, use functions like massErase and execute without any problems  (All these over UART). Now my MCU needs the nBOOT0 option bytes to boot correctly.

I have tried several times with the STMCubeProgrammer API function "sendOptionBytesCmd" but it does not work. I always get a "-6" as return value. Does anyone have an idea how to solve this ?

This is what my code looks like.

qDebug() << "Setting Option Byte nBOOT0 to 1";

int sendOptionBytesCmdFlag = sendOptionBytesCmd((char*)"-ob nBOOT0=1");
if (sendOptionBytesCmdFlag ! = 0) {
disconnect();
qDebug() << "Could not set Option Byte nBOOT0 to 1";
}

qDebug() << "Option Byte nBOOT0 set to 1 successfully! " << sendOptionBytesCmdFlag;

Thanks in advance :)

4 replies

Amine_Jridi
Technical Moderator
May 16, 2025

Hello @csmk59,

I have added your code into the UART example on QT API project with an STM32G474 and it works well on my end. Could you provide more information about your setup? exact part number of your STM32G4? CubePorgrammer version and any additional details (logs, UART configuration...).

Thanks,

Amine.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Amine_Jridi
Technical Moderator
June 3, 2025

Hello @csmk59,

Any feedback?

Thanks,

Amine.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
csmk59Author
Associate
June 5, 2025

Hi  @Amine_Jridi 

Sorry for the late reply.
The exact name of my MCU is “STM32G431CBY3TR.”.

I even have the latest version of the STMCube32 Programmer API. That didn't work either.
There aren't many log files. As I said, everything works except for setting option bytes. Sometimes I get -1 as the return value or even -6. I don't understand.

This is how the UART connection was established.

usartConnectParameters port{"", 115200, EVEN, 8, 1.0f, OFF, 0, 0, 0, 0, 0};

As I said before, Firmware download, chip erase, everything works perfectly.

Regards,

Claude

Amine_Jridi
Technical Moderator
June 24, 2025

Hello @csmk59,

 

I have attempted to reproduce the issue you described, but everything is functioning correctly on my side.

To help you better understand the error codes, please refer to the API documentation available at:

> /Path/To/CubeProgrammer/API/doc

 

In particular, the return value -6 corresponds to CUBEPROGRAMMER_ERROR_INTERFACE_NOT_SUPPORTED, which means that the interface is either not supported or not implemented on this platform.

 

Thank you,
Amine

 
In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.