(SOLVED) STMH7A3ZI-Q. No STM32 target found. ST-link working.
I received my stm32h7 nucleo board yesterday. It worked fine with StmCubeProgrammer and uploaded multiple programs on it but from today I can not connect my board to Cube programmer.
The error code I am receiving is given below :
00:00:22 : STM32CubeProgrammer API v2.9.0
00:00:22 : ST-LINK error (DEV_CONNECT_ERR)
00:06:14 : ST-LINK SN : 002C00483038511834333935
00:06:14 : ST-LINK FW : V3J9M3
00:06:14 : Board : NUCLEO-H7A3ZI-Q
00:06:14 : Voltage : 3.26V
00:06:14 : No STM32 target found!
00:06:14 : ST-LINK SN : 002C00483038511834333935
00:06:14 : ST-LINK FW : V3J9M3
00:06:14 : Board : NUCLEO-H7A3ZI-Q
00:06:14 : Voltage : 3.26V
00:06:14 : Error: No STM32 target found!
Things I have tried but was unsuccessful:
*Reinstalling everything, drivers included.
*Using a different windows computer.
*Tried hardware button reset then connecting.
*Tried ST-link Utility
*Tried to erase full chip also erase all sectors
*Different cables
*Powering it externally
*Tp1 measures 3.3v and tp2 is 1.8v
*Tried connecting an FTDI usb-uart board to the D0 and D1 pins.
*Changing the frequency and reset mode.
*Upgrading the st-link FW
I have multiple stm32f4 boards and non of those ever acted this way. I am at a loss now. Refunding is not an option unfortunately. I do not have a ST-Link. But I do have st-link enabled nucleo boards. I do not have any jtag accessories only have ftdi usb-uart boards.
I would be extremely grateful if someone could help me with this. I have searched the net for solves but nothing works for me.
Regards
Wahid
Edit- Solved it by connecting BT0 to VDD and erasing the chip. Should have read the user manual first before panicking !